What should be done if the control voltage for the heater circuit must be 240VAC rather than the standard 120VAC.
Two heaters must be wired in series to drop 120VAC across each hearter. They must be placed in the switchgear so that the correct wattage is provided in each section
CTA-ID : 2018667
CTA-ID : 2018667
Answers which others found helpful |