Are replacement contacts available for the Class 2510 / 2511 / 2512 Type M & T manual starters?
Yes, in three pole kits only. Select based on size of controller from below:
For Types MB & TB = 9998ML1
For Types MC & TC = 9998ML2
Note: Class 2511 & Class 2512 devices include two manual starters and therefore two kits wil be required.
CTA-ID : 4441
For Types MB & TB = 9998ML1
For Types MC & TC = 9998ML2
Note: Class 2511 & Class 2512 devices include two manual starters and therefore two kits wil be required.
CTA-ID : 4441
Answers which others found helpful |