What communications protocol options are available for the Altivar ATV58?
FIPIO, MODBUS/UNITELWAY, INTERBUS S, MODBUS PLUS, PROFIBUS DP, DEVICE NET, ETHERNET MODBUS TCP/IP, LONWORKS to MODBUS and JOHNSON CONTROLS N2 are the communications we have at this point.
There may also be some 3rd party gateway or bridge solutions for other protocols.
For example Panel-tec offers a bridge for Siemens P1 protocol. This device is not directly supported by SquareD-Schneider Electric. However, we can assist with the settings that involve the drive Modbus communications to this device.
CTA-ID : 6857
There may also be some 3rd party gateway or bridge solutions for other protocols.
For example Panel-tec offers a bridge for Siemens P1 protocol. This device is not directly supported by SquareD-Schneider Electric. However, we can assist with the settings that involve the drive Modbus communications to this device.
CTA-ID : 6857
Answers which others found helpful |