FAQ Search

Are the IEC K-Line contactors SEMI F47 compliant?

K-Line contactors are SEMI F47 compliant. Additionally, the addition of an overload relay makes them SEMI F47 compliant motor starters.

The K-Line offering is available in 6 amp and 9 amp versions for SEMI F47 when used with 24 and 120 volt ac control coils. All DC controlled versions are SEMI F47 compliant as standard.

All K-Line products carry the UL, IEC and CE markings. For additional information and other products for SEMA F47 applications refer to the attached link.



CTA-ID : 2017163
FA109027  |  18-Jun-2012  | Codes/Std/Certification
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful