What is option code B08 on a 883958E Econoflex unit?
It is a light cluster option for Red Power On / Green AFC Run / Yellow AFC Fault / Yellow Bypass
CTA-ID : 2014874
FA107886 |
14-Jan-2011
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> Can the option C08 ( light cluster Red power on, Green AFC run & Yellow AFC Fault ) be used with the A07 ( Hand / Off / Auto , Speed Potentiometer) on the 883958E?
> What is the part number for the optional line reactor mounted internally on the 1-25hp ATV58 Econoflex drives?
> Why does unit with the V2.0 Powersuite software get an error message indicating problems with the TCP/IP port? The error reads as follows. ``It is impossible to launch the TCP/IP server of configuration. Please check that the protocol TCP/IP well is installed and active on the PC or if another Powersuite application is in course of execution.``
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel