Will the HOMRBGK2 generator interlock kit work on the RC816F200C combination devices?
NO. Use the RCGK2 generator interlock kit which is design for the combination Service Entrance devices ONLY.
CTA-ID : 2015190
FA107760 |
14-Jan-2011
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> Is a bypass provided on the RC816F200C Combination Service Entrance Device ?
> What type of branch circuit breakers are used with the RC816F200C Combination Service Entrance Device ?
> Are Generator Kits available for CSED devices?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel