FAQ Search

I want to upgrade a Powerpact P frame breaker from a Micrologic 3.0 to the 5.0P 6.0P 5.0H or 6.0H trip units. How do I get the voltage sensing needed to calculate power?

When a P frame breaker is ordered with the P or H trip unit, you get internal voltage sensing. When upgrading to the P or H trip unit, an external voltage sensing kit must be installed.
Part numbers for field installable external voltage sensing kits are as follows:
S64203 EVS kit P frame unit mount / I-LINE
S64208 EVS kit R frame unit mount / I-LINE
S64209 EVS kit P frame drawout
S64210 EVS kit P frame motor operated / rotary handle


CTA-ID : 2013879
FA107233  |  14-Jan-2011  | Inoperative
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful