FAQ Search

How many Micrologic A, P or H trip units can be supplied with an auxiliary power supply 24 VDC ?

That depends on the power supply. The trip unit requires 100 mA @ 24 Vdc.
So a 5 VA power supply @ 24 V (5 VA / 24V = 0.208 A) could supply two trip units.
The Phoenix power supply provided with Columbia switchboards has an output of 2.5 A, and could feed as many as 25 trip units.


CTA-ID : 2013287
FA106765  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful