FAQ Search

Can a Powerpact R frame breaker with a basic Micrologic trip unit (3.0) be upgraded to a type A, P, or H trip unit?

Yes. In addition to the new trip unit, a 12 pin connector (Cat. no. S33100) must be purchased.

It is essentially the same as S33101 (used on NT an NW) less the 4 inch wires and black plugs, but with additional terminal marking on the block.


CTA-ID : 2013265
FA106419  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful