FAQ Search

What is the maximum QO or QOB branch breaker (not sub-feed brkr) that can be installed in an NQOD panelboard?

The maximum QO branch breaker that can be installed in an NQOD panel is a 2-pole 125Amp. The maximum QOB branch breaker that can be installed in an NQOD panel is a 2 or 3 Pole, 150Amp.


Revised 5/5/04






CTA-ID : 2012061
FA105620  |  14-Jan-2011  | Application
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful