FAQ Search

How is PI control enabled in the ATV58 for setpoint control?

Set AI2 in menu 5 (I/O menu) for PIF.
This function is available after enabling the Variable torque Macro and ensuring that the Auto/man (RFC) parameter is not assigned to a logic input.
Once set for PIF, this automatically sets AI1 for the setpoint and activates the PI settings in menu 2 for adjustment and tuning as desired.
See the Altivar 58 keypad programming guide for more information.


CTA-ID : 2008225
FA103423  |  29-Jul-2012  | Adjustments
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful