How does a QORBGK2 Generator Interlock Kit function?
This interlock kit provides an interlock bracket between the QOM2-VH main breaker (Utility Main) and a back-fed, 2-pole QO (125 ampere maximum) branch circuit breaker (Generator Main). This interlock bracket will allow only the Utility Main breaker or the Generator Main breaker to be in the ON position at any time. The bracket manually slides between the handle of the Utility Main breaker and the handle of the Generator Main breaker, not allowing them to be in the ON position simultaneously.
CTA-ID : 2007608
CTA-ID : 2007608
Answers which others found helpful |