FAQ Search

How does a HOMRBGK2 Generator Interlock Kit function?

This interlock kit provides an interlock bracket between the QOM2-VH main breaker (Utility Main) and a back-fed, 2-pole HOM (125 ampere maximum) branch circuit breaker (Generator Main). This interlock bracket will allow only the Utility Main breaker or the Generator Main breaker to be in the ON position at any time. The bracket manually slides between the handle of the Utility Main breaker and the handle of the Generator Main breaker, not allowing them to be in the ON position simultaneously.


CTA-ID : 2007610
FA102365  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful