If you manually push the test button on a solid state overload relay , should it trip the motor?
Yes. If the unit does not trip, it is wired incorrectly or is not functioning correctly.
CTA-ID : 2007548
FA102153 |
14-Jan-2011
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> What is the indication of a flashing or blinking LED on the Motor Logic solid state overload relay?
> What are the main differences between the melting alloy and Motor Logic solid state overload relays?
> Can you manually test trip the Class 9065 Type SS***, Type SR***, Type SF*** or Type ST*** solid state overload relay?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel