FAQ Search

What load centers are compatible with the HOMRBGK2 Generator Interlock Kit?

The HOMRBGK2 is compatible with any Series S2, outdoor, single phase, convertible main breaker Homeline load center that utilizes a QOM2 frame main circuit breaker (150 - 225 ampere). It interlocks the QOM2 2-pole main circuit breaker with a back-fed HOM 2-pole (15-125 ampere) branch circuit breaker. A retaining means is also provided for the back-fed HOM branch breaker.
NOTE: Series S2, convertible Main Lug Only load centers, that meet description provided above, could also be used by converting the load center to a Main Breaker device.


CTA-ID : 2006354
FA101847  |  14-Jan-2011  | Application
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful