Is there a mechanical interlock for the 8910DP and 8910DPA definite purpose contactors?
No, consider the Class 8965 or Class 8702 product offering.
CTA-ID : 2002775
FA101226 |
14-Jan-2011
|
Product Features
PDF
Email
Bookmark
Print
Answers which others found helpful
> Is the form `U1` still available for the Series C, 8910 contactors (20-40A).
> Are the 8910 definite purpose contactors provided with quick connect terminals?
> What is the replacement coil for 8910DPA43V02, Series C.
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel