FAQ Search

Can an electronic trip circuit breaker be used to protect conductors with ampacity less than the sensor size of the breaker?

Yes.
Per NEC 240.6-c: A circuit breaker(s) that has restricted access to the adjusting means shall be permitted to have an ampere rating(s) that is equal to the adjusted current setting (long-time pickup setting). Restricted access shall be defined as located behind one of the following:
(1) Removable and sealable covers over the adjusting means
(2) Bolted equipment enclosure doors
(3) Locked doors accessible only to qualified personnel




CTA-ID : 2004255
FA100082  |  14-Jan-2011  | Codes/Std/Certification
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful