Is there a mechanical interlock for a QO 3 pole breaker?
No. Available to 1 and 2 pole QO breakers only.
CTA-ID : 2000965
FA98543 |
25-Jun-2012
|
Selection
PDF
Email
Bookmark
Print
Answers which others found helpful
> Do we have a Mechanical interlock, like the QO2DTI, but for 3-pole QO breakers??
> What is the range of QO breaker amperages that can be interlocked with a QO2DTI Mechanical Interlock Attachment?
> Customr needs Mechanical Interlock Attachment for interlocking the handles of two 2- Pole or one 2- Pole and one 1- Pole QO and Q1 breakers mounted side-by-side so that only one breaker can be ``ON`` at a time
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel