FAQ Search

Are NEMA 1 enclosures offered for encapsulated transformers for indoor applications?

An encapsulated transformer is offered with a standard NEMA 3R rated enclosure which is suitable for both indoor and outdoor applications.


CTA-ID : 2000141
FA98014  |  18-Jun-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful