FAQ Search

Can multiple motor leads fed from AC Drives share a conduit or raceway?

It is not recommended that output cables from different AC drives share close proximity in raceways or conduits. Because of the high frequency switching and increased capacitance, the drive may fault under some conditions. Damage to the drive and/or motor may result from disregarding this recommendation.

For example, see page 39 of the manual VD0C06S304E. Similar wording is found in many other publications


CTA-ID : 13180
FA96087  |  18-Jun-2012  | Wiring
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful