FAQ Search

What are the repair parts for UFP222R, Series G02, AC Disconnect?

THE Pullout - 4050711750  IS OBSOLETE AND NO LONGER AVAILABLE
Only the parts listed below are considered field replaceable (for pictures see attached link):
Interior Trim - Cannot be provided due to UL labeling issues.
Pullout - 4050711750 (This pullout will work for either Series G01 or G02)
Interior Trim Mounting Screw  4020513001K (This kit includes 10 screws. Only one screw is required)


CTA-ID : 2056705
FA152199  |  08-Aug-2012  | Maintenance
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful