FAQ Search

What is the differences between the EZM31200GCBU and EZM31200GCBE Main devices?

The EZM31200GCBU is a Underground ONLY feed, non-EUSERC, that comes standard with lugs.
The EZM31200GCBE is a Underground ONLY feed, meets the EUSERC standards and does NOT come standard with lugs, but has Lug Landing Pads for lugs to be purchased separately and installed in the field.
Each device has the same Frame main breaker, but different catalog numbers with different connection types. (SEE CAD DRAWING FOR LUGS SIZES and MAIN BREAKER CATALOG NUMBERS).


CTA-ID : 2060281
FA149425  |  23-Jul-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful