What is the part number for the field installable Start Stop button for a NEMA 7 & 9 Enclosure?
Field addition of pilot lights, push buttons or selector switches CANNOT be done for any Class 8502 or Class 8536 NEMA 7 & 9 Cast Iron Enclosures . This is because the holes required for these operators are not drilled unless they are ordered when the starter is manufactured.
Also, the enclosure only is not available as a repair part.
CTA-ID : 2060209
Also, the enclosure only is not available as a repair part.
CTA-ID : 2060209