What is the torque requirement for lugs for the Powerpact L frame breaker?
The torque requirement for the following lugs is 50 N-m or 442 lb.-in.
AL400L61K3, AL600LS52K3, CU600LS52K3, AL600LF52K3, CU600LF52K3
The torque requirement for lug CU400L61K3 is 31 N-m or 275 lb.-in.
CTA-ID : 2059561
AL400L61K3, AL600LS52K3, CU600LS52K3, AL600LF52K3, CU600LF52K3
The torque requirement for lug CU400L61K3 is 31 N-m or 275 lb.-in.
CTA-ID : 2059561
Answers which others found helpful |