Can LDR raintight wireway be cut to lenght in the field ?
This cannot be field cut. By doing so will affect the raintight rating.
CTA-ID : 2055006
FA131086 |
14-Jan-2011
|
Assembly/Installation
PDF
Email
Bookmark
Print
Answers which others found helpful
> Can I use LDR type wireway with conduit to individually mounted meterbases? Does this product line have conduit holes pre cut?
> Are end caps required for NEMA 3R Raintight Wireway such as catalog number RDB65?
> Can NEMA 3R wireway be mounted vertically and keep the NEMA 3R rating?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel