FAQ Search

To add a CE3090B to an existing NHDP panel?

The CE3090B breaker is obsolete, as are the CE3090E CE3090N and CE3090H Breakers.
There are no replacement breakers or hardware available to mount alternative breakers in the NHDP panels.

Suggested alternative panel is the Square D NF panel.


CTA-ID : 2053882
FA130168  |  14-Jan-2011  | Cross Reference
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful