FAQ Search

How is the equipment ground path established when connecting multiple cabinets of EZ Meter-Pak metering equipment to one another?

EZ Meter-Pak meter equipment is UL Listed in File E131840 as a Modular Panelboard and complies with UL50, UL67, and UL414.
Refer to the attached  bulletin #: 73293-715-01 Installation Step #7 for the procedure to properly bond one cabinet to the next within a meter center lineup using three points of contact, with three captive screws and three 1/4``20 nuts provided, torque each to 50 lb-in (do not over tighten).
NOTE: Bonding of Panelboard cabinets do not comply with the Bonding approach taken for multi-section Switchboards.



CTA-ID : 2035172
FA121749  |  29-Jul-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful