FAQ Search

Can the factory installed 400A DJM circuit breaker as used in EZML and EZMK branch units be adjusted for other ampere ratings?

The DJM32400E20 circuit breaker is used for both 3-Phase and 1-Phase (connects to two outside poles only) applications.
This 400A circuit breaker is supplied with an adjustable AMPERE RATING feature ranging from 160A minimum to 400A maximum.
A Tamper-evident seal kit for this DJM breaker is available by ordering catalog number: 29375.  The kit meets NEC 240-6(c) requirements.
Refer to the attached document for details on how to dial-down the ampere rating of this circuit breaker.


CTA-ID : 2034683
FA120945  |  25-Jun-2012  | Application
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful