FAQ Search

Are the F-Line contactors rated to break DC voltages?

Yes, 125 VDC per pole which means that through a four pole device breaking 500 VDC is possible by wiring all four power poles in series. However, be aware that the device current ratings will differ according to the number of poles in series and the type of application.

Devices are suitable but not UL Listed for DC applications.

See pages 28 through 31 of the attached link (8502CT9901R5/03)


CTA-ID : 2027003
FA116383  |  29-Jul-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful