FAQ Search

ATV58 What is the range for the analog output for motor power based on?

On this parameter OPr, the maximum value is 200 % of the nominal power of the drive based on the Constant Torque Ratings for most ATV58 drives. For The ATV58HC10N4 and larger, it is 200% of the nominal power of the drive based on the Variable Torque Ratings.


CTA-ID : 2026313
FA115084  |  23-Jul-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful