Can a Model 6 LVMCC unit be installed in a Model 5 LVMCC section?
Yes, a Model 6 unit can be installed in a Model 5 section with the proper mounting hardware. Note that a Model 6 unit, except a Compac 6 (6`` unit) cannot be installed in the space directly below a Model 5 top shelf. When placing an order, provide the existing Model 5 LVMCC factory order number (found on the UL structure nameplate label). See the document link for the instruction bulletin.
CTA-ID : 2024162
CTA-ID : 2024162
Answers which others found helpful |