FAQ Search

What is the largest branch breaker that can be installed in an NF panel?

125 amps, E(D,G, or J)B34125.  A 250 amp max sub feed breaker can be installed as a factory assembled option or with the addition of a sub feed breaker kit.

The largest single pole breaker is 70A.



CTA-ID : 2022228
FA112480  |  09-Jul-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful