How do you field convert the 8903 Type L or Type LX power contacts from normally open to normally closed?
See contact conversion steps listed in the attached instruction bulletin.
CTA-ID : 2019389
FA110570 |
02-Jul-2012
|
Assembly/Installation
PDF
Email
Bookmark
Print
Answers which others found helpful
> Are 8903 type L & LX power contacts convertible in the field from normally open to normally closed and vice versa?
> Can the 8903 L and LX contacts be individually converted from normally open to normally closed or must all contacts be changed?
> 8903L: How does he change the contacts from NO to NC?
Please rate the content of this information
Unhelpful
1
2
3
4
5
Helpful
What can we do to improve this information?
.
Your email address
> Submit Feedback > Cancel