FAQ Search

What are the specifications for the R1 and R2 relays in the ATV58 drive?

R1A to R1C is a normally-open (N.O.) contact. When the drive controller is powered with no fault, the contact is closed.
R1B to R1C is a normally-closed (N.C.) contact. When the drive controller is powered with no fault, the contact is open.
The R2 relay is a normally opened (N/O) programmable relay.
The relays have a switching capacity as follows:
Minimum:  10 mA for 24Vdc
Maximum inductive load of 1.5 A for 250Vac and 30Vdc
Maximum resistive load 5 A for 250 Vac and 30 Vdc


CTA-ID : 2015918
FA108275  |  29-Jul-2012  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful