FAQ Search

Are replacement DC bus capacitors available for the ATV58 drive?

It depends on the part number for the drive.
The ATV58HC10N4XZU and larger drives have replacement DC bus capacitors available. See the installation guide for details.
There are no DC bus caps available for the Altivar 58 drives smaller then the ATV58HC10N4. If the DC bus capacitors are dammaged, the drive should be sent in to SquareD for depot repair or replacement.


CTA-ID : 2013091
FA106527  |  29-Jul-2012  | Selection
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful