Can a Square D encapsulated transformer with a style A, B, or C enclosure be wall mounted?
Wall mounting is the standard mounting method for all Square D encapsulated transformers in style A, B, or C enclosures as noted on page 12-8 of the Digest 172. Larger, custom quoted and built encapsulated transformers (37.5 through 75kVA 1ph and 45 through 225kVA 3ph) are floor mounted as standard, and are typically not wall mounted to the extreme weight of larger encapsulated transformers. Contact Product Marketing/Support via the Field Office for assistance with larger encapsulated transformer questions.
CTA-ID : 15953
CTA-ID : 15953