FAQ Search

Can Class J fuses be used with a 600 ampere Heavy Duty safety switch?

Yes. An adaptor kit, catalog number H600J, is also required. One adaptor kit required per 3 pole switch. With Class J fuses installed, the switch is UL Listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.


CTA-ID : 2002603
FA99606  |  14-Jan-2011  | Application
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful