FAQ Search

What are the repair parts for the H664DS, series F5? (may be shown as F05)

The repair parts for the H664DS, series F5 (F05) are as follows. No other parts are available.
Complete Line Base - 4056703850 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 40205-142-02 (requires 12 per line base)
Load Base Assembly - 40566-782-50 (requires one per phase - includes phynolic base, lugs and fuse clips)
Load Base mounting screws - 40205-142-02 (requires 2 per load base)
Arc Suppressor Assembly - 40566-775-50 (requires one per phase)
Arc Suppressor mounting screw - 40205-145-01
Lug Assembly - CL20F (incl. 6 lugs - requires mounting screws below)
Lug Assembly mounting screw - 21401-222-40 (per lug)
Switch Mechanism - 40567-401-50 (also requires mechanism coupling assembly 40566-998-50 and interlock connector assembly 40567-188-50)
Switch Mechanism mounting screws- 21949-181-21 (requires 2)
Handle Assembly - 40567-368-50
Lockplate - 40567-389-01
Lockplate mounting screws - 21949-181-21 (requires 2)



CTA-ID : 8950
FA93444  |  14-Jan-2011  | Maintenance
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful