Does the EV230PSRR charging station use any energy when in the standby mode? In other words, when no vehicle is being charged?
Yes, a very minimal amount of energy is used when the charger is in standby mode. In normal ambient temperature (25 Deg C/77 Deg F) and normal voltage (240Vac) the charging station uses 1.85 Watts of energy. The wattage is calculated based on a current draw of 0.0163 Amps at 240Vac, Power Factor of 0.47.
CTA-ID : 2060002
CTA-ID : 2060002