FAQ Search

What is the NEMA rating or IP degree of protection for the door-mounted 32598 RE12 and 32600 RE22 rotary handle operator for the Powerpact D frame (and NSJ) breaker?

32598 and 32600 are IEC-Style Door-Mounted Rotary Operating Handles.  The handle mechanism can be used in NEMA 3R and 12 enclosure applications.  Degree of protection: IP40 per IEC 529.


CTA-ID : 2059919
FA144520  |  30-Apr-2012  | Codes/Std/Certification
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful