FAQ Search

What is the maximum current rating for the spade or quick connect terminals on the Class 8910 Type DP & Type DPA contactors?

30 amps, 75 degree Celsius conductor.


CTA-ID : 2025011
FA114716  |  14-Jan-2011  | Product Features
  • Please rate the content of this information
    Unhelpful 1 2 3 4 5 Helpful