FAQ Search

What is the standard sound level (in dB) of Transformers of various kVA ratings?

Issue:
Sound level can be a factor when specifying Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Transformers of different kVA sizes can generate varying levels of sound when energized

Resolution:
Square D/Schneider Electric Transformers are built to standard sound levels listed in NEMA Standard ST-20.  The transformers and corresponding sound levels per NEMA ST-20 are as follows . These can also be found in the Digest :

         kVA <> NEMA standard sound level
         0 - 9 <> 40dB
     10 - 50 <> 45dB
   51 - 150 <> 50dB
 151 - 300 <> 55dB
 301 - 500 <> 60dB
 501 - 700 <> 62dB
701 - 1000 <> 64dB


CTA-ID : 2033247

FA120629  |  12-Feb-2014  | Application
Please rate the content of this information
Unhelpful star.gif 1 star.gif 2 star.gif 3 star.gif 4 star.gif 5 Helpful
What can we do to improve this information?
Your email address