FAQ Search

What is the DC Bus voltage trip threshold for ATV31?

Overvoltage Trip
For drives with part numbers ending in M2, M2A, M3, or M3A DC bus voltage overvoltage level is 400 VDC.
For drives with part numbers ending in N4 or N4A the DC bus voltage overvoltage level is 840 VDC.


CTA-ID : 2024469
FA114168  |  14-Jan-2011  | Product Features
Please rate the content of this information
Unhelpful star.gif 1 star.gif 2 star.gif 3 star.gif 4 star.gif 5 Helpful
What can we do to improve this information?
Your email address