FAQ Search

What is the difference between Variable Torque and Constant Torque for AC Drive ratings?

Issue:
Explanation of the difference between Variable Torque and Constant Torque for AC Drive ratings

Product Line:
All Altivar ATV drives.

Environment:
All

Cause:
Application notes about VT and CT loads.

Resolution:


VARIABLE TORQUE LOADS:
Many types of loads require reduced torque when driven at speeds less than the base speed of the load. Conversely, such loads may require increased torque when driven at speeds greater than the base speed of the load. These are classified as variable torque loads. Many variable torque loads decrease with the square of the speed. This is characteristic of centrifugal pumps, and certain types of fans and blowers. Typically, as the speed decreases, the torque decreases with the square of the speed and the horsepower decreases with the cube of the speed.

CONSTANT TORQUE LOADS
With constant torque loads, the torque loading is not a function of speed. Typical applications are: Traction drives, Conveyors, Positive displacement pumps and Hoists. As the speed changes, the load torque remains constant and the horsepower changes linearly with speed. Constant torque loads cause motors to draw relatively high current at low speeds when compared to variable torque applications. This is why the same size drive may have a lower HP rating for Constant Torque applications.

CTA-ID : 2011978


 

FA105387  |  17-Jan-2014  | Application
Please rate the content of this information
Unhelpful star.gif 1 star.gif 2 star.gif 3 star.gif 4 star.gif 5 Helpful
What can we do to improve this information?
Your email address