{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.

Search FAQs

How do you wire for 480V - 120/240V on 1 phase S3 type transformer (e.g. EE37S3H)?

Article available in these languages: Spanish

Issue:
Single Phase Transformer Primary and Secondary wiring

Product Line:
LV Transformers

Environment:
Applies to Energy Efficient (EE) type Transformers by SquareD/Schneider Electric

Cause:
Transformers are delivered in an unconnected condition, and must be configured for the system need.


Resolution:
Connect a jumper between the H2 and H3 terminals, and bring the 480V in on H1 & H4. Do not connect any inputs to the H2/H3 connection
Connect a jumper between the X2 and X3 terminals. This will serve as the neutral, and can be bonded to ground, if permitted or required by local code. There will be 240V between X1 and X4 with 120V between X1 and the X2/X3 junction and 120V between X4 and the X2/X3 junction. Again, X2/X3 will be the neutral.  Be sure to check with local Electrical Inspectors or Authority Having Jurisdiction (AHJ) for direction about grounding transformers in your local area.

Schneider Electric USA

Attachment(s)

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.