Search FAQs
PowerLogic PM5000 Series (PM5100, PM5300, PM5500) Installation and User Guide
Issue
PM5000 Series Installation and User Guide
Product Line
PM5110, PM5330, PM5340, PM5560, and PM5563
Environment
Installation, Datasheet, Configuration, Programming, Instruction bulletin, User Manual
Cause
Documentation is needed to configure and install a PM5000 series meter
Resolution
View attached User Guide and Installation Guide below for PM5100, PM5300, and PM5500 series meters.
Refer to Article FA234024 for Technical datasheet, Brochure, and Part number breakdown.
Refer to Article FA234017 for Register List. Note this can be also found under each new firmware folder released from the SE website (se.com).
PM5000 Series Meter Documentation (Technical datasheets, Instruction sheets, and User guides)
Note:
If the inside FAQ link is not opening but global window popping up, please proceed as the following or copy it and open it a new window:
PM5000 Series Installation and User Guide
Product Line
PM5110, PM5330, PM5340, PM5560, and PM5563
Environment
Installation, Datasheet, Configuration, Programming, Instruction bulletin, User Manual
Cause
Documentation is needed to configure and install a PM5000 series meter
Resolution
View attached User Guide and Installation Guide below for PM5100, PM5300, and PM5500 series meters.
Refer to Article FA234024 for Technical datasheet, Brochure, and Part number breakdown.
Refer to Article FA234017 for Register List. Note this can be also found under each new firmware folder released from the SE website (se.com).
PM5000 Series Meter Documentation (Technical datasheets, Instruction sheets, and User guides)
Note:
If the inside FAQ link is not opening but global window popping up, please proceed as the following or copy it and open it a new window:
- Click on the hyperlink like “FA234024”,
- (1) The global window “Select Location for FAQ” appears,
- (2) Select your location,
- (3) Then select your Country,
- then the hyperlink article will open.
Released for:Schneider Electric USA
Attachment(s)
Explore more