Search FAQs
Is there a GFI option for the breakers used in the NF panelboards? (EDB, EGB, EJB)
Issue:
GFI option for the breakers used in the NF panelboards (EDB, EGB, EJB).
Product Line:
NF Panelboards, E Frame Circuit Breaker
Environment:
Products sold in North America
Resolution:
The EDB, EGB, and EJB circuit breakers do not come with a GFI option for people protection at 4-6mA protection. They are only available with equipment ground-fault protection at 30mA (EPD). These are only available in single-pole.
Note: NF EPD circuit breakers cannot be used on phase to ground less then 277V. These breakers are not suitable for a 208Y/120V application.
GFI option for the breakers used in the NF panelboards (EDB, EGB, EJB).
Product Line:
NF Panelboards, E Frame Circuit Breaker
Environment:
Products sold in North America
Resolution:
The EDB, EGB, and EJB circuit breakers do not come with a GFI option for people protection at 4-6mA protection. They are only available with equipment ground-fault protection at 30mA (EPD). These are only available in single-pole.
Note: NF EPD circuit breakers cannot be used on phase to ground less then 277V. These breakers are not suitable for a 208Y/120V application.
18 ka @480Y/277 Vac | 35 ka @480Y/277 Vac | 65 ka @480Y/277 Vac | |
15 A | EDB14015EPD | EGB14015EPD | EJB14015EPD |
20 A | EDB14020EPD | EGB14020EPD | EJB14020EPD |
30 A | EDB14030EPD | EGB14030EPD | EJB14030EPD |
40 A | EDB14040EPD | EGB14040EPD | EJB14040EPD |
50 A | EDB14050EPD | EGB14050EPD | EJB14050EPD |
Released for:Schneider Electric USA
Explore more
Explore more