Applications

Use the select and go menu below to view case histories of Schneider Electric Material Handling applications.

 

Carousels

A Vertical carousel consists of trays that travel vertically in front of an access window. One or several chains drive the trays, which are arranged according to the nature, dimension, and weight of the item to be stored. Read more...

Overhead Conveyors

A chain carries running trolleys on a suspended rail, and is driven by one or more motor-reduction units. Equally-spaced hooks on this chain are used to suspend the loads. Read more...

Automated Storage and Retrieval Systems

The transtorage system consists of a self-propelled column moving along a central aisle (traverse). It supports a vertically sliding platform (lifting). Read more...

Lifting Platforms

The lift table brings loads to level by action on one or several hydraulic jacks pushing against one or several systems. Read more...