Time-to-Market
Construction phase - shorter time-to-market
Schneider Electric goes beyond on-time delivery of world class products to reduce your time from plant layout to production.
- The Design Resource Center is a 24/7 compliment to the expertise of local sales engineers to help you design world class industrial facilities
- Even before your order is finalized, PMI certified project managers start work to assure effective coordination between you, other key value chain members, and our global manufacturing organization. Installation is fast and easy, because the products are designed with installation in mind.
- The Model 6 iMCC reduces installation time and costs by replacing large bundles of field-control wiring with either pre-wired I/O or networking technology. Total installed cost-savings generally average 10% to 30%
- New NQ panelboards are the state of the art in lighting panelboard design.
- I-Line® panelboards are the most versatile power distribution panelboard on the market
- I-Line® busway offers versatility in application and a simplicity in installation that cable and conduit can't match
- Our comprehensive start-up and commissioning services assure your new electrical equipment is energized safely and extends the warranty of some products