Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image

Product Support Resources


                        Advantys STB Modular Distributed I/O Platform


                        Savings and reliability in one compact system

                        The Advantys STB provides a distributed I/O platform by delivering a wiring solution, power management and device integration system all in one compact device. As open modular IP20 distributed I/O platform, the Advantys STB is a cost-effective, feature rich distributed I/O solution that places I/O at the point of control to provide a 60% savings in wiring and installation costs with improved reliability and operation.